Data Service
Virtual EMpro REST API
In this no-code environment, you can explore the features of the EMpro REST API. Interact with the host www.empro.phoenixcontact.com, where a virtual device is updating values every 1 s. Reduce your development effort by clicking the send button. Read electrical quantities, read device information, control the tariffs or reset meters. Also, read from the historical recordings. The responses are just a click away.
Start now
Zwei Menschen besprechen die Anforderungen an die Datenintegration in einer Werkhalle

How to use

Click on example request to get a frequency value from the virtual device.

GET

GET a collection of items in one single request

All measurements

GET

All meter readings

GET

All device information

GET

GET Measurements

GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET

GET Meter Readings

GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET

Control | Reset Meters

Check example meter before and after reset

GET

Then send reset command here:

PUT

Control | Change Tariff Number

GET

Change tariff number here:

PUT
PUT
PUT
PUT
PUT

Read Information

GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET
GET

Historical Data Access

All examples were requested at T12:35:53Z

Call the last 10 recordings at T12:35:53Z. The period is 5 minutes. The end of the intervals is synchronized to the internal clock time. The first record is from T12:35:00Z

GET

Call the last 4 recordings at T12:35:53Z. The period is 30 minutes. The end of the intervals is synchronized to the internal clock time. The first record is from T12:30:00Z

GET

Call the last recording at T12:35:53Z. The period is by default 15 minutes. The end of the interval is synchronized to the internal clock time. The first record is from T12:30:00Z

GET