EMS On-Premises Help Center


Installation of the Software


Installation of EMS Executing the Installation on a UPC

In this video you see the explanation how the software is installed at the UPC 2440 Edge Computer from Phoenix Contact. The same way can also be used at a server or other computers.

Licensing of EMS Licensing the installed software

In this video you see how a license for EMS is set on the UPC or other systems. The license is activated at an offline UPC – just like in the most applications. Updating a license requires the same steps.

Operation of the Software


Software Overview A fly through of current functions

In this video you see our Dashboards, Charts Section, Configurations like Calculations, Importers and Dataobjects as well as Reports in a short overview of our ISO 50001 certified software.

Starting and setting up the software First Startup

In this video you can see the initial setup of the software - valid from version 1.2.0. The setup is guided from the first login and the integration of measuring devices to the first view of a dashboard and the control of the existing values.

Dashboard settings Change the Dashboards and their information

In this video you see how the different Dashboards can be freely named and the information in them is set. Also the timeframe which data is visible is explained.

Configurable Charts Section New Chart Section from Release 1.1.0

In this video our new Charts Section from Release 1.1.0 is shown. Different Dashboards can be created individually including period comparisons and heatmaps.

PDF Reports New PDF Reporting from Release 1.2.2

In this video you can see how a Chart is turned into a PDF Report. The Report can be executed just once or also several times and sent via email automatically.

Import Modbus Data Using an Importer

In this video you can see how its possible to include any device via Modbus/TCP. You can include our MID meters and other meters on the market. Additionally you can add values of our EMpro, that are not already included automatically (like Current or Voltage values)

Import CSV Data And how to save CSV files on the EPC

In this video you learn how to import CSV files. CSV files can for example handle constants for calculation, measurement data from any device or production data.

Create new Users And change user rights

In this video you learn how to create and change users. It includes filtering dataobjects for different users, setting email filters and set a password.

Calculations and Summations Create calculations and new values

In this video we create a summation of different dataobjects. Also other calculations are possible like subtraction or divisions.